an engineer works on the atlas robot

Innovation at Boston Dynamics

Boston Dynamics has a long history of leadership in the robotics field, pushing the boundaries of the possible and creating robots smart and capable enough for the unstructured world. Explore our history of R&D, innovation, and inspiration.

Inside our Robotics & AI Research

Our robots aren’t designed overnight—our R&D teams have spent countless hours testing and iterating on new builds or ideas. Get to know the team behind the machine.

Three Decades of Robotics

The foundation of today’s portfolio: Our future is built on the groundwork of our previous research. Each of Boston Dynamics’ legacy robots has contributed towards crucial milestones in the advancement of applied robotics and our current products.

Our History Through The Years

2023

Hydraulic Atlas

The hydraulic Atlas pushed the limits of dynamic motion and manipulation.
  • Powerful parkour and dance
  • Whole body control algorithms
  • Manipulation of heavy and irregular objects

1/2
2017

Handle

Handle served as a research venture into wheeled robots.
  • Led to the development of Stretch
  • Truck unloading and pallet building
  • Dynamic balance on two wheels

Handle 1st
1/3
2015

Spot Classic

Spot Classic laid the groundwork for the agility and compactness seen in Spot today.
  • Quadrupedal movement
  • Indoor and outdoor operation
  • Boston Dynamics’ first fully electric robot

1/3
2011

Wildcat

WildCat was built for speed, making it the fastest quadruped robot on Earth.
  • 19 mph on flat terrain
  • Dynamic balance
  • Variable gait and mobility options

2012

Sandflea

Earning its moniker, the compact, 11lb Sandflea was built to vault high in the sky.
  • Capable of jumping 30ft in the air
  • Remote controlled
  • Built-in stabilization system

1/2
2010

LS3

LS3 (Legged Squad Support System) was a rough-terrain robot with significant carrying capacity.
  • 400 lbs of payload
  • Could travel 20 miles before refueling
  • Sensors for navigating obstacles 

2007

RHex

RHex was a 30lb, six-legged robot designed for mobility on rough terrain. 
  • Operated remotely 
  • Could travel upside down
  • Rugged construction

1/2
2006

RiSE

RiSE was a six-legged robot designed to climb without any special adhesion.
  • Lightweight with strong legs
  • Each foot consisted of approximately 50 fishing hooks
  • Climbed at a rate of 5 cm/s

1/2
2004

BigDog

BigDog was our first legged robot to leave the lab.

  • Navigates rough terrain
  • Sensor and control system
  • Dynamic balancing

1/3
See the products delivering on our history of innovation.
Take the first step to build the next chapter at Boston Dynamics.

Join our mailing list

Sign up to receive the latest developments from Boston Dynamics