Inspection
Blogs •
Distribution centers, manufacturing plants, corporate campuses, and other facilities are turning to robotics to support their perimeter security operations.
This article was written by Ryan Hodgens, application expert at Asylon Robotics. Asylon is an American manufacturer and service provider for security drones and robotics.
Mobile robots like Spot are starting to become more commonplace, automating industrial inspections in factories and helping emergency responders safely assess hazardous scenarios from a distance. However, there are also thousands of distribution centers, manufacturing plants, corporate campuses, and other high-value facilities that are in need of cost-efficient and effective security solutions.
Security has become an increasing focus and concern across industries over the last several years. For example, incidents of cargo theft have been rising consistently over the last several years, increasing 15% year-over-year in 2022. Moreover, security jobs can be some of the most dangerous, with security guards facing some of the highest risks for both workplace homicides and non-fatal workplace violence of any profession. Drones and robots can be incredibly useful technology to augment efficiency and effectiveness while minimizing risks for security professionals.
Robotic perimeter security is the process of securing a facility perimeter with aerial drones or ground robots to safeguard people, places, and property. Because site security is so critical to employee safety and business operations, it requires constant vigilance. Robots can help add necessary coverage without further taxing on site personnel. Typical customer goals when deploying robotic security solutions is to increase site security, employee safety, and operational efficiencies.
Before continuing on, it’s important to recognize that perimeter security is an exceptionally demanding use for robots and drones. In addition to requiring a higher threshold of patrol consistency and reliability to perform the regular site checks, these sites often require navigating over curbs, unstructured terrain, and in dynamic environments. Despite the demanding nature that can come with leveraging robots for perimeter security, there is a major need.
Safe and secure places for people and property should be the standard. Yet, they’re often taken for granted and require diligent work. With nationwide staffing shortages, extremely high annual turnover rates, and significant workplace risks to officers, a full-service solution with agile, mobile robots like Spot is key to achieving safety and security standards at scale.
Additionally, while AI and robotics are useful to automate routine rounds, effective security programs require reacting to emerging situations with intelligence, critical thinking, and empathy. People can and should be in the loop; remote monitors and on-site staff can work collaboratively and both be a core part of robotic perimeter security. This blend of human expertise with advanced robotics and AI is not only a core enabler of the technology today but also creates significant upskilling opportunities.
There are three primary applications for security robots:
Each of these applications serves a specific purpose. To accomplish each of these, reliability, availability, and remote operability are required due to the demanding nature and often high stakes involved with perimeter security.
Robotic perimeter security is an effective addition in many organizations’ security infrastructure, driving consistency and transparency while also extending the reach of other security tools and staff. The benefits can include:
With more than 70,000 miles patrolled at customer sites to date, Spot robots are actively operating for customers like Moderna, GXO Logistics, and Mercedes-Benz Stadium. At the Mercedes-Benz Stadium in Atlanta, for example, the robot works alongside the security team by patrolling the graveyard shift in an area of the stadium complex that’s open to the public. The live video stream is monitored remotely and site activity is reported in real-time for consistent patrolling and enhanced employee safety. Greg Overstreet, the senior director of stadium security for Mercedes-Benz Stadium, has stated, “Since the implementation of DroneDog in our Home Depot Backyard, not only have we seen occurrences of theft and vandalism drop to zero but we have also increased safety for our employees.” From our experience, companies using this technology today are seeing a decrease in theft and vandalism, while also experiencing an increase in operational efficiencies.
To operationalize robots at scale, we’ve found that the best approach for our customers is to adopt a full-service model. This full-service combination of robots, people, and software has led to the successful completion of more than 100,000 security missions with the Spot robot, demonstrating an exponential growth trend as we operate 24/7 for an increasing number of customers.
By managing the program in this way, we’ve experienced a greater flexibility in service and support as well. In cases where a deployed robotic asset requires maintenance, the Asylon operations team will promptly ship a replacement robot from our larger fleet to the site and it will be met by a field technician to resume operations as quickly as possible. This approach helps ensure the highest possible uptime for the program, which is critical for effective perimeter security.
To learn more, see how Asylon completed 100,000 missions with Spot.
At Asylon Robotics, our primary application is perimeter security. We’ve taken the Spot platform and developed a complete, turnkey robotic security solution. From our 24/7 Robotic Security Operations Center (RSOC), we’ve completed over 70,000 miles of remote operations with Spot robots and more than 40,000 missions with our aerial security drone-in-a-box system. Asylon, an American manufacturer and service-provider, has built the only full-service aerial and ground-based robotic perimeter security solution.
Recent Blogs
•55 min watch
Leveraging Robotics for Smarter Perimeter Security Inspections
•42 min watch
Spot’s Formula for Success
•4 min read
An Ethical Approach to Mobile Robots in Our Communities
Have a question about our robots and applications? We're here to help. Reach out to our sales team to learn how advanced mobile robots can impact your operations.